Dear B&R Support Team,
I have a NanoTech drives, When moving the motor using ‘Absolute Move’ or ‘Jog Pos/Neg’, the motor only moves briefly before an error occurs.
This is my SM1444-1 Motor Controller Card, We configured the current to 1.8 A according to the NanoTech motor Configuration. We are using McAxis Library and McAxisBasic FB
We configured the motor as such :
We checked precisly the motor hardware connection, The voltage inserted is 4.8 V which is suitable to our Nanotec motor according to the specification sheet, We can power the motor and can also Home it, If we disabled the Encoder. To motor rotates fine, but the issue arrises when we enable one Encoder, if we set a position and a velocity from MpAxisBasicParType
If I command something like MoveAbsolute, or JogPositive, after enabling one Encoder, the motor will move a little bit till it reaches Position of 5.002001 and then Error will be True then i will need to Reset the Error
Till now i couldn’t find the reason of the error and i couldn’t diagnose it. I searched in this Community and in Automation Help but the information are very limited, I will be glad to get support and guidance from your side of from any memeber who encountered this before and know the solution
I have attached the relevant log data and screenshots to this Post. The first Log is for when i try to Jog positive the motor the second is for MoveAbsolute Command, basically both trigger the same Error then the Axis FB will be switched off
JogPosLog.logpkg (19.5 KB)
MoveAbsLog.logpkg (26.5 KB)
Just inform me if you need further details.
Thank you in advance for your assistance.