APROL Report printing in Web portal

Good Morning,

Has anyone come across this error before when trying to print reports in the web portal? We have printer setup and can print from a file etc. Using this print icon on the report gives the

following error. This is the same if we use the report as embedded or in a window.

Any help or ideas would be greatly appreciated,

Regards,

Dale Webb

Hi @martin.schmollngrube, maybe you can help here?

Hi @Dale_Webb
First of all it would be interesting to know more about your APROL system. For example the release version.
HTTP error 501 means “not implemented”.
I am not aware of a known issue but if such a basic function ends in a “not implemented” of the web server, I would guess it could be a bug.
So I would first check, depending on your APROL Release, if there is a patch available and install it.
If problem persist please go through proper APROL support channel.
Hope this helps you!

Good Morning,

We are running Patch 4.4-00P6

We don’t get the same error on our other system which is an older Patch 4.4-00P3 which is configured almost identically. So maybe this could be a Patch issue?

Kindest Regards,

Dale Webb