Hello there,
I am currently playing around with the simulating capabilitys of AR Sim as part of writing a bachelors thesis on drivetrain simulation. Right now i have a simple setup of one acopos beeing connected to a single motor. My next step would be to introduce simple loads while tracing speed, power and torque. From what i have gathered from my reasearch and testing, torque and power are either positive or negative infinity when i have the one mass load model configured on the Acopos.
I have limited Automation Studio Experience and i am completly new to simulating with AR Sim althought i have spend a couple of days tinkering with getting my first simulation to run without immediately running into a drive error. Mapp Cockpit also already works for me. Im either getting the same readings i am with tracing in AS or straight up errors. (Traces in mapp cockpit are marked with a red exclimation mark)
I believe that for actual torque readings i have to implement additional function blocks. From my reasearch i have gathered additional librarys are in need for this. One of those library would be MTMpcSiso, that is sadly still in development as far as i can tell. This entry supports this Can't find MTMpcSiso for Automation Studio 6 .
I would really appreciate if anyone had any good information on a basic setup, or a simple project with a working simulation like this one from Loupe in AS 4 https://www.youtube.com/watch?v=v-ZJCO9ORd8&t=5s
I am aware of both Acopos for Simulink and B&R Target for Simulink librarys. Licenses are already in the work. In the meantime i want to find out as much as i can about the simulating capabilitys within AR SIM.
Appreciate every bid of help ! Thanks in Advance
-Malte