ARsim Startup won't startup at all

Hi,

I have an reocurring issue, where ARsim won’t startup and only shows this error in the logs:

$arlogsys:EventID -2147453618 (WARNING, 0, 30030), lpBin=0x08f8fe5c, "PnPManager", "SS1.IF1"
$arlogsys:EventID -2147453618 (WARNING, 0, 30030), lpBin=0x08f8fe5c, "PnPManager", "SS3.IF1"
$arlogsys:EventID -1073716425 (ERROR, 0, 25399), lpBin=0x00a5dc98, "ArException", ""

I had it one time where I could fix it by copying InaFrms.dll into the folder of the ar000loader.exe of the simulated PLC.

Has anyone ever seen this isse? I can’t find any help for this online.

It’s also strange that I could click “Exit ARSim” in the windows tray icon, but the ar000.exe and ar000loader.exe are not killed and still visible in the taskmanager.

I also don’t get any errors in the ar000log.txt:

Thu Oct 15 15:17:07 2026
COPYRIGHT (C) B&R Industrial Automation GmbH

Thu Oct 15 15:17:07 2026
No ARsim registration found!

Thu Oct 15 15:17:07 2026
InstanceName: 000000007aee74f5

Thu Oct 15 15:17:07 2026
WorkingDirectory: C:\Simulation\

Thu Oct 15 15:17:07 2026
COMMAND_COLDSTART

Thu Oct 15 15:17:10 2026
Version: P4.93

I hope someone can help me out :smiley:

Greetings

Hi @SantasKleinerHelfer

Welcome to the community!

I remember to have similar issue, I don’t really remember the exact AR version, but I see that you are using P4.93 version of AR.

Did you already try to upgrade AR to a newer version?

That was my solution!

Regards,
Florent

Hi Florent,

I need a bit more help, can I find the newest version online? I’m quite unfimilar with the ARSim, to be honest :smiley:

Greetings

The ARSim version is the same that you configured in the project for the Automation Runtime.

You can check in Project–>Change Runtime Version…, in the popup you can change the Automation Runtime version based on the different version already install on your system.

If you need to get more version or newer you can check in the Tools–>Upgrades… popup to download and install newer version of Automation Runtime.

Regards,
Florent

Unfortunately I don’t have access to the PLC projects. I get the finished PLC simulation projects from our PLC developers.

Currently I had PVI 4.12.4.36 installed, I tried to upgrade to 4.12.11.3 (Latest from homepage) but somehow this installer won’t do anything.

I open the installer, click language, install and then the installer is blocked and does not respond at all :man_shrugging:

Can I use the PVI 6.7.0 (also latest on homepage) instead? Why are there 2 major release versions of PVI online and PVI 4.12.4.36 has a newer timestamp?

Ohh you don’t have access to the PLC projects. You have to ask your PLC developers to change the AR version and regenerate the ARSim to give it to you!

For PVI versions there is 2 major versions of Automation Studio (the PLC developement software), but vers 4.12 is long time support so there is still new release on this.

But I would recommend to use the same version that you have on ARSim!

I found it out! It was the .NET version!

I’m a C# dev, so I had several versions on my machine and it seems that ARSim took a version that was not compatible.

I installed the latest .net10 sdk 10.0.402 and uninstalled all older versions (.net8 sdk, runtime, 3.1 sdk) and now it works, woho! :smiley: