Hello,
I am maintaining a Genius 52 printing press manufactured in 2003, equipped with a B&R System 2005 control system.
The machine is currently operational and my primary goal is to create a safe disaster-recovery backup before making any changes to the PLC.
Hardware
- B&R System 2005
- CPU: 3CP260.60-1
- Power supply: 3PS465.9
- Interface module: 3IF672.9
- Interface module: 3IF681
- Original PCMCIA memory card is installed
- Existing Ethernet connection between IF681 and the machine HMI
- CPU RS232 interface available
Problem
I need the Automation Studio 2.7 Base Installation.
I can find the AS 2.7.0.25 SP18 upgrade, but I cannot obtain the original AS 2.7 Base Installation Medium.
I specifically need the Base Installation, not only the SP18 upgrade.
Backup question
I do not have the original Automation Studio source project.
Before attempting any programming or modifications, I would like to make the safest possible complete backup of the running 3CP260.60-1 / SG3 system.
I found information on this Community that Runtime Utility Center can be used to backup/restore SG3 targets, even though the original editable source project cannot be recovered from the PLC.
Could someone please advise:
-
Can someone from B&R provide the Automation Studio 2.7 Base Installation Medium?
-
For backup only, would Runtime Utility Center (RUC) be a better/safer choice than Automation Studio?
-
Which version of Runtime Utility Center / PVI should be used with a 3CP260.60-1 System 2005 SG3 target?
-
Can the complete executable application, Automation Runtime and configuration be backed up over the CPU RS232 interface and later restored to an identical 3CP260.60-1?
-
Is there a recommended procedure/document for creating a full disaster-recovery backup of a CP260 without modifying anything on the running PLC?
-
Is there any additional backup procedure recommended for the original PCMCIA memory card?
The machine is currently running correctly, so my priority is read/backup only. I do not want to perform a download, Automation Runtime update, memory initialization or any operation that could modify the existing PLC until a verified backup exists.
Any help from someone experienced with System 2005 / SG3 / CP260 would be greatly appreciated.
Thank you.