B&R X20 I/O Modules Remain Dark After Cabinet Power Cycle

We have an Alfa Laval separator control panel with a B&R X20CP0292 CPU and X20PS9500 power supply module.

After switching the entire cabinet off and back on, the following modules remained completely dark:

  • A7: X20AI4622
  • A8: X20AT2222
  • A10: X20DI4760

The preceding modules still show green LEDs.

For troubleshooting, we swapped only the electronic modules A7 and A3 (X20DI6371). Both showed flashing green LEDs in the exchanged positions. However, after restoring the original arrangement, A7 remained completely dark. Swapping a bus base with another matching base did not resolve the issue.

Could this indicate a loss of internal I/O supply, an X2X communication issue, or another fault? Which voltage measurement points and diagnostic checks would you recommend

Hey Hyssein, Welcome to the community.

No led at all normally means no power at all on the x2x and IO. The weird part is that you are able to switch 2 of them and they work.

I don’t know if you tried that but could you unplug the terminal block and only the terminal block on the last 3 module while the machine is powered down and restart the machine?

If they are green after that, there is probabably an electrical problem somewhere on those cable.

Hello,

if you only Switch Off the Cabinet and Switch On the Cabinet. I would normaly don’t think of
a mechanical issue of “lose contacts” But you can try to unmount the whole modules
A7, A8, A9 once an remount them correctly.

The System is build of three Parts. Shown in Picture.
The Contacts between the Modules are interconecting them and are marked.

If the Electronic Module of A7 worked in A3 Position, we can assume the Module is fine.
In this case i would recomment to exchange the X20BM11 behind the A6 (Sender side of issue) or A7 (Reciver side of Issue).

Greetings
Michael

Good morning

Thank you for your suggestion. I have already tried disconnecting only the terminal blocks from A7, A8, and A10 with the power off, then restoring power, but the modules remained dark. I also replaced the bus bases for A6 and A7, but the issue persists

I swap the A3 to A7

Hi @Hussein36 what is status of your issue, can you update us?

Good morning

After check again the problem come from connection between models I check again and connected, now the system working good

Thanks for supporting

Hey Michael,

the top voltage is not 24V-IO, that is the X2X voltage (~5V).

Best Regards,

Lukas

Hello Lukas,

Thanks for the hint, i have modified the picture.

Greetings
Michael