siddique
(muhammad siddique)
April 10, 2026, 2:40am
1
hi,i have one windmoller and holscher printing machine,during machine running there Can bus Error come.but when see PLC there no
show.but screen show and machine stop.this machine used x20 cp3583 2 plc and
x20 cp 3585 2 plc communication card x20 if 2772.all plc look like ok
after few minutes machine power off than ON back every thing normal.
can any bidy inform me what is reason.
thanks.
eun.im
(Eun Im)
April 10, 2026, 4:37am
2
Hello Muhammad,
Welcome to join our community.
The LEDs only indicate the basic status.
For more detailed information, you can download and analyze the system dump.
If the current hardware LED status is normal but the equipment has stopped, the equipment operation sequence should be analyzed.
In this case, I’m recommend contacting the machine manufacturer.
Best regards
Eun Im
kovarj
(Jaroslav Kovar)
April 10, 2026, 5:01am
3