Error while creating a offline Installation - AS 4.11


Has anyone faced this problem creating an offline Installation?
I have even tried creating a new installation via RUC Package but still the same error.

Hi and welcome!

I haven’t had this error on my own, but from the message I would recommend to check:

  • a different card reader, if possible β†’ the usb card reader could cause a timeout for the drive access
  • temporary deactivation of antivirus β†’ a AV scan/intervention could interrupt the (low level) access to the card
  • start Automation Studio explicitly with admin rights (right click β†’ run as administrator) β†’ missing right could prevent the build, especially building the partition table + formatting

Best regards!

I have also seen issues where some other automation vendor software captures control of CF and CF readers. For that vendor it was possible to store licensing information, like a dongle, on a CF/CFast card. Once i killed that vendors licensing process in windows task manager, i was able to use the CF adapter connected to the laptop.

Thanks for the suggestions. i need to start Automation studio or the .pil file as Administrator and then it works.