I tried to load the EDS file to AS, but it won’t let me add the device to eth2, I get this message: It is not possible to connect hardware module CJ2M-EIP21 V2.1 to connector IF4 of 5PPC2100_BY01_000, because there is no fitting connector on CJ2M-EIP21 V2.1.
Any suggestion?
About the library, is there any manual or tutorial to use it?
I’m not familiar with EthernetIP, but as I remember AsEthIp is an implementation based on a standard ethernet interface of a PLC, therefore EDS files aren’t usable for this library.
To use EDS files, you need an additional dedicated EthernetIP interface.
Some information about AsEthIp can be found in the Automation Help:
The mentioned sample should be part of the Automation Studio installation.