How to read temperature from ACOPOS servo drive

Hi everyone,
Could you please describe me the procedure how to read
temperature of the motor from Servo drive ACOPOS.
Motor is connected to servo drive with encoder EnDat2.2
What i need to read and from where?
I use NC mapping Acp10map.
Iv seen something about ParID 381, but i don’t know where to read that, which function to use.

Thanks. Marko

Hello,

if you really need the value in your application code consider using function blocks:

MC_BR_CyclicRead

or

MC_BR_ReadParID

381: Temperature sensor: Temperature

let us know why you need it, please

Hello,

costumer want the temperatures showed on the HMI.

Hello,

thanks, got it.

Of course, every read operation consumes resources on the Powerlink network, so you should use them sparingly.

Well, I think the client really only needs this information every few minutes, so I would trigger the read operation using MC_BR_ReadParID every few minutes.

I’d also like to mention that there is an motor temperature model, which is used for monitoring (and shutting down the axis).

393: Motor: Temperature model: Temperature