Hi,
I need a TCP functionality on a machine using 4 axis CNC block. The machine is a needle winder, with a nozzle. The nozzle has a tilting possibility (0 to 90 deg)
When a pusher rod is actuated (by servo motor on ball screw), the tool holder rotates from 0 to 90 deg using a crank mechanism. See the below picture for an idea.
To keep the Tool Centre Point constant in space, the Nozzle Bar X axis and Y axis need to be compensated in upwards and rightward directions.
Is there any standard functionality in B&R to achieve TCP constant in space for this custom mechanism?
We are currently doing it approximately by another (not so reliable & slow) method. See working video of machine in Youtube - Needle Winder
The have the related mathematical transformation equations ready with values. I am just looking for a method to implement it on B&R.
- The CNC blocks we use are MpCnc4Axis block.
- The drive system is an ACOPOSmulti with 8LS servomotors.
Thanks in advance!!
Thanks @kovarj. Look forward to your suggestions.
If 4ax CNC XYZC is configured according to a picture above, i.e. vertical X and left-right Y, then a movement of C programmed like G01 G91 C90 shall produce required circular movement of QX and QY (such a movement could represent approx. 20th-22nd second of the linked youtube video). For sure, it is necesary to properly configure especially location of QC and the Flange, event. the TCP.
Alternatively, one could think of using another 4ax CNC variant if it suits better the machine layout (XYZA, XYZB and XYZC are supported by mapp Motion).
Hi @zbynek_uher thanks for this. But I have an issue here.
My machine will have a total of 5 ax on CNC. X, Y, Z for Nozzle Linear axis. QC to Rotate the Nozzle. Additionally, I need also an Indexer in the same axial axis as QY from below image.
I also explored the 5 axis CNC (XYZBA & XYZCA). But both these configurations have the BA and CA axes coupled and inter-related. Is this possible to change in the configuration to make it independent? If yes, I can try this configuration as a 5 axis CNC.
Please bear with my questions, I don’t use BR AS directly (I am a Mechatronics Engineer) but my role is to provide a direction in which my team of programmers / automation engineers need to work towards to achieve the required functionality.
Some additional information, the movement of the X axis as per my old drawing or QY as per current CNC wire frame - will not be a straight light, it is a curve like shown below approximately in order to keep the TCP constant in space.
The vertical axis needs to following positions like below:
- Little more than 15mm at 0 deg.
- Reaches peak of 25+mm at approximately 55 deg.
- Then comes down to 20mm at 90 deg.
The Y axis as per my old drawing or QX as per current CNC wire frame will move is a straight line (B&R community didn’t allow me to attach a 3rd image in the same post). Please see next post.
Thanks in advance for any ideas.
Warm Regards!!
The Y axis as per my old drawing or QX as per current CNC wire frame will move is a straight line
Well, if any of 4ax CNC is used, then one must work with revolute axis C (drawn in red).
Once its conversion to some linear move is needed (e.g. drawn in blue), it is a non-linear transformation, therefore a coupling between joints in the axis group is not an option. One needs to make this conversion in an application, or through single axis coupling (cam). A dependency is not too complex, actually it is the same like a dependency between TCP.Z coordinate and a joint coordinate e.g. in 2-ax delta during the simple Z-movement (both joints move the same).
One could also think about custom mechanical system in our axis group which can work with any number of axes you need. Equations for direct and inverse transformation functions and their derivatives must be prepared but as an advantage, one does not have to build some additional logic above the 4ax CNC in the application.
Thankyou for the suggestions @zbynek_uher . Will try them out.