# Is it possible to activate variable forcing (ForceActivated / ForceActivated Value) programmatically via PVI?

**URL:** <https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377>\
**Category:** Programming\
**Tags:** pvi\
**Created:** [March 4, 2026, 9:29am UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377 "2026-03-04T09:29:21Z")\
**Posts on this page:** 10\
**Page:** 1

<div class="post-metadata">

**Author:** ![Johan\_Elfing](https://avatars.discourse-cdn.com/v4/letter/j/FF8800/32.png) [@Johan\_Elfing](https://community.br-automation.com/u/Johan_Elfing)\
**Post date:** [March 4, 2026, 9:29am UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/1 "2026-03-04T09:29:21Z")

</div>

Hello,

I am currently developing a Python-based framework for a B&R PLC application using **PVI** to communicate with the controller.

For the Python side I’m using the wrapper Pvi.py: [GitHub - hilch/Pvi.py: Python wrapper for B&R Pvi (process visualization interface) · GitHub](https://github.com/hilch/Pvi.py) .

Through PVI I can successfully read and write process variables using the Python wrapper (`pvi.Variable`). For example:

```auto
var = Variable(task, "AF_AI[6].ModuleOk")
var.value = True

```

However, the variable is overwritten again during the next PLC cycle because it is updated inside a cyclic task (100 ms). In Automation Studio I can solve this manually by enabling **ForceActivated** and setting **ForceActivated Value** in the watch window.

![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/0/08b6ae81c562c5399da73d754ecbe6981e02ccc8.png)

What I would like to do is **activate this forcing programmatically via PVI** , similar to what Automation Studio does when clicking “Force”.

So my questions are:

1. Is it possible to activate **ForceActivated** and set **ForceActivated Value** through PVI?

2. If so, which PVI API or command should be used to do this?

Currently the `Variable` object in the Python wrapper exposes attributes such as:

```auto
value
status
descriptor
readable
writable

```

but I do not see any methods related to forcing.

If forcing cannot be controlled via PVI, what would be the recommended approach for automated testing in this situation?

Thanks in advance for any guidance.

---

<div class="post-metadata">

**Author:** ![alexander.hefner](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/alexander.hefner/32/111_2.png) [@alexander.hefner](https://community.br-automation.com/u/alexander.hefner)\
**Post date:** [March 4, 2026, 9:37am UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/2 "2026-03-04T09:37:31Z")

</div>

Hi, and welcome to ourCommunity!

Yes it’s possible, but I’m not sure if it’s already integrated into the Python wrapper (I don’t think so).

In general, forcing of IO variables can be done with PVI DLL interface (which is also used by the Python wrapper) by accessing the so-called “link nodes” (via the ANSL variable object):

> **[B&R Online Help](https://help.br-automation.com/#/en/6/automationnet%2Fpvibase%2Flines%2Flnansl%2Fpvilnansllinknode.htm)**

Additionally, forcing is also possible directly inside the PLC code by using the [AsIO](https://help.br-automation.com/#/en/6/libraries/asio/asio.html) library functions:

- [AsIOEnableForcing](https://help.br-automation.com/#/en/6/libraries/asio/fbks/asioenableforcing.html)
- [AsIODisableForcing](https://help.br-automation.com/#/en/6/libraries/asio/fbks/asiodisableforcing.html)
- [AsIOGlobalDisableForcing](https://help.br-automation.com/#/en/6/libraries/asio/fbks/asioglobaldisableforcing.html)

Best regards!

---

<div class="post-metadata">

**Author:** ![Johan\_Elfing](https://avatars.discourse-cdn.com/v4/letter/j/FF8800/32.png) [@Johan\_Elfing](https://community.br-automation.com/u/Johan_Elfing)\
**Post date:** [March 4, 2026, 3:02pm UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/3 "2026-03-04T15:02:31Z")

</div>

Hi,

Thanks for the quick response.

I’ll investigate this further. If the Python wrapper doesn’t solve the problem, I’ll likely proceed with the alternative solution you suggested.

Best regards,  
Johan

---

<div class="post-metadata">

**Author:** ![christoph.hilchenbac](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/christoph.hilchenbac/32/423_2.png) [@christoph.hilchenbac](https://community.br-automation.com/u/christoph.hilchenbac)\
**Post date:** [March 5, 2026, 9:02am UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/4 "2026-03-05T09:02:30Z")

</div>

Hi,

with PVI (and Pvi.py) it is possible to write to the force value (‘F+’ syntax).

 ![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/d/d20bafcf34b310f019647f5af329e390860c7a20.png)

It is also possible to read the status of the forcing with [POBJ\_ACC\_STATUS](https://help.br-automation.com/#/en/6/automationnet/pvibase/core/pvicomrequrespaccesstype.htm%23pobj_acc_status).

 ![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/0/0cebd74a3a81ab415c4229bb0d489b9c10a202f4.png)

 ![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/6/68e59f2b8ce8889e25db4d8f69080a78cdd43d11.png)

Unfortunately it is not allowed to change (e.g. to write to) the forcing status.

To my knowledge, forcing can only be enabled with Automation Studio (and by the FB Alex mentioned), but I’m happy to be corrected.

Find example attached.

[linknode.txt](https://community.br-automation.com/uploads/short-url/xg2Tn2BhO3nPIHd8mUoYURVilKr.txt) (1.5 KB)

---

<div class="post-metadata">

**Author:** ![Johan\_Elfing](https://avatars.discourse-cdn.com/v4/letter/j/FF8800/32.png) [@Johan\_Elfing](https://community.br-automation.com/u/Johan_Elfing)\
**Post date:** [March 9, 2026, 2:22pm UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/5 "2026-03-09T14:22:20Z")

</div>

Hi Alexander,

Do you know if it’s possible to activate **“ForceActivated”** using the **AsIO library**?  
If so, do you happen to have an example of how to do it?

---

<div class="post-metadata">

**Author:** ![christoph.hilchenbac](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/christoph.hilchenbac/32/423_2.png) [@christoph.hilchenbac](https://community.br-automation.com/u/christoph.hilchenbac)\
**Post date:** [March 9, 2026, 2:30pm UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/6 "2026-03-09T14:30:16Z")

</div>

> Do you know if it’s possible to activate **“ForceActivated”** using the **AsIO library**?

if you mean how to get the status of forcing: use [AsIODPStatus()](https://help.br-automation.com/#/en/6/libraries/asio/fbks/asiodpstatus.html)

---

<div class="post-metadata">

**Author:** ![Johan\_Elfing](https://avatars.discourse-cdn.com/v4/letter/j/FF8800/32.png) [@Johan\_Elfing](https://community.br-automation.com/u/Johan_Elfing)\
**Post date:** [March 9, 2026, 2:38pm UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/7 "2026-03-09T14:38:21Z")

</div>

I wanna activate the “ForceActivated” according to the picture. This is the last piece of the puzzel, the rest I have implemented / figure out.

Currently using: AsIOEnableForcing.

![ForceActivated](https://europe1.discourse-cdn.com/brcommunity/optimized/2X/f/f0254d58b5b66869ba22cb65833f449841c46416_2_690x52.png)

---

<div class="post-metadata">

**Author:** ![alexander.hefner](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/alexander.hefner/32/111_2.png) [@alexander.hefner](https://community.br-automation.com/u/alexander.hefner)\
**Post date:** [March 9, 2026, 2:55pm UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/8 "2026-03-09T14:55:38Z")

</div>

Hi @Johan_Elfing,

as Christoph mentioned, you can query the force status by AsIODPStatus(), the FB output “.flags” contains this information:

 ![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/d/d31bcc4a782aad985a4f959356b8c75890bb73b3.png)

---

<div class="post-metadata">

**Author:** ![christoph.hilchenbac](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/christoph.hilchenbac/32/423_2.png) [@christoph.hilchenbac](https://community.br-automation.com/u/christoph.hilchenbac)\
**Post date:** [March 10, 2026, 11:37am UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/9 "2026-03-10T11:37:48Z")

</div>

> [@Johan\_Elfing](#):
>
> Currently using: AsIOEnableForcing.

to our knowledge that is exactly the way you have to follow.

Either use Automation Studio or this function block.

---

<div class="post-metadata">

**Author:** ![Johan\_Elfing](https://avatars.discourse-cdn.com/v4/letter/j/FF8800/32.png) [@Johan\_Elfing](https://community.br-automation.com/u/Johan_Elfing)\
**Post date:** [March 16, 2026, 9:07am UTC](https://community.br-automation.com/t/is-it-possible-to-activate-variable-forcing-forceactivated-forceactivated-value-programmatically-via-pvi/10377/10 "2026-03-16T09:07:11Z")

</div>

Thanks alot for the help I made it work :).  
@alexander.hefner @christoph.hilchenbac