I am facing an intermittent axis fault on a machine using a B&R ACOPOS P3 drive with 8EAC0122.001-1 Resolver Interface Module.
Issue Description
- During motor start, the axis trips with the following errors:
- 29214
- 7032
- 5034
- Initially, these errors would occur occasionally, and after a reset the machine would run normally for some time.
- Recently, the fault has become more severe:
- After the error occurs, a power cycle does not clear the fault.
- The same errors remain active after reboot.
- After approximately 5-6 hours, the errors clear automatically and the axis operates normally again.
Hardware
- Drive: ACOPOS P3
- Resolver Module: 8EAC0122.001-1
- Feedback: Resolver
Request
Has anyone experienced a similar issue with these fault codes on an ACOPOS P3 drive?
I would appreciate any suggestions regarding:
- Resolver feedback issues
- Resolver module failure (8EAC0122.001-1)
- Encoder/resolver cable problems
- Motor resolver faults
- Drive hardware faults
- Recommended diagnostics to identify the root cause
Thank you in advance for your support.