# Multi-core Functionality

**URL:** <https://community.br-automation.com/t/multi-core-functionality/7474>\
**Category:** B&R Software & Runtime\
**Tags:** automation-studio-6\
**Created:** [July 3, 2025, 2:47am UTC](https://community.br-automation.com/t/multi-core-functionality/7474 "2025-07-03T02:47:46Z")\
**Posts on this page:** 5\
**Page:** 1

<div class="post-metadata">

**Author:** ![Black\_Cho](https://avatars.discourse-cdn.com/v4/letter/b/FF8800/32.png) [@Black\_Cho](https://community.br-automation.com/u/Black_Cho)\
**Post date:** [July 3, 2025, 2:47am UTC](https://community.br-automation.com/t/multi-core-functionality/7474/1 "2025-07-03T02:47:46Z")

</div>

Dear Community,

Hello. I’m writing to the community because I’m curious about the multi-core functionality in Automation Studio 6. The help documentation is a bit lacking, so I have a few questions:

1. For hypervisors, when multi-core settings are enabled, is multi-core configuration possible?
2. When multi-core settings are enabled, do features like Mapp View or other functions improve?
3. Does the functionality improve only on PLCs like the X20CP0410 without Powerlink?
4. In version 6.2, when testing with and without multi-core settings, there was no difference in CPU load in SDM. Is there a separate way to verify this difference?

Thank you in advance for your response.

---

<div class="post-metadata">

**Author:** ![tommi.piiparinen](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/tommi.piiparinen/32/2183_2.png) [@tommi.piiparinen](https://community.br-automation.com/u/tommi.piiparinen)\
**Post date:** [July 3, 2025, 5:19am UTC](https://community.br-automation.com/t/multi-core-functionality/7474/2 "2025-07-03T05:19:48Z")

</div>

Hello,

> [@Black\_Cho](#):
>
> For hypervisors, when multi-core settings are enabled, is multi-core configuration possible?

Multi-core configuration is not yet supported when using hypervisor. The feature is under development and will come available in a later version of Automation Runtime.

> [@Black\_Cho](#):
>
> When multi-core settings are enabled, do features like Mapp View or other functions improve?

Depending on multi-core settings it is possible to move the workload to multiple cores, which should improve the performance.

> [@Black\_Cho](#):
>
> - Does the functionality improve only on PLCs like the X20CP0410 without Powerlink?

X20CP0410 does not have multiple cores, so the setting has no effect. (If configured for multi-core on a single-core target system only a single core is used).

> [@Black\_Cho](#):
>
> In version 6.2, when testing with and without multi-core settings, there was no difference in CPU load in SDM. Is there a separate way to verify this difference?

SDM and/or Profiler can be used to determine the effect. Which PLC did you use to test it? If it only has one core there is no difference to see.  
[Automation Help: Profiler](https://help.br-automation.com/#/en/6/diagnostics_support/diagnosis/profile/diagnosis_profile.html)

---

<div class="post-metadata">

**Author:** ![Black\_Cho](https://avatars.discourse-cdn.com/v4/letter/b/FF8800/32.png) [@Black\_Cho](https://community.br-automation.com/u/Black_Cho)\
**Post date:** [July 3, 2025, 6:24am UTC](https://community.br-automation.com/t/multi-core-functionality/7474/3 "2025-07-03T06:24:20Z")

</div>

> [@tommi.piiparinen](#):
>
> Depending on multi-core settings it is possible to move the workload to multiple cores, which should improve the performance.

Tommi Piiparinen,

Thank you for your response.

Hardware : X20CP0484

I have a few questions.

Currently, I am using VC4 HMI for testing purposes, and the motion is set up with a 2-axis SDC configuration. In this case, when I enable or disable multicore, there is no change in the usage of Core 0 and Core 1. Are there any additional settings that need to be configured?

---

<div class="post-metadata">

**Author:** ![corne.geerts](https://avatars.discourse-cdn.com/v4/letter/c/FF8800/32.png) [@corne.geerts](https://community.br-automation.com/u/corne.geerts)\
**Post date:** [July 3, 2025, 6:58am UTC](https://community.br-automation.com/t/multi-core-functionality/7474/4 "2025-07-03T06:58:22Z")

</div>

The X20CP0410 is a dual core cpu and also benefits from the multicore functionality.  
See following post: [Multi-core support since AS\AR V6.1](https://community.br-automation.com/t/multi-core-support-since-as-ar-v6-1/5949)

---

<div class="post-metadata">

**Author:** ![tommi.piiparinen](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/tommi.piiparinen/32/2183_2.png) [@tommi.piiparinen](https://community.br-automation.com/u/tommi.piiparinen)\
**Post date:** [July 3, 2025, 8:56am UTC](https://community.br-automation.com/t/multi-core-functionality/7474/5 "2025-07-03T08:56:52Z")

</div>

Ah… My bad on the number of cores, thanks for correcting Corne!