No sources can be selected on the Permanent variable page in AS6.7.0.187


Hi @jianing.kang ,
I did a small test with X20CP1686X, AS 6.7, AR 6.7:

In my case it works.

Which CPU do you have?
Are your variables global and retain?
Have you configured a memory size for permanent variables on your CPU?

Ciao
Valerio

X20CP3687X; AR6.7.6

yes,Absolutely, that’s definitely the root cause. I’m not new to B&R development. The variables I’m using are global and retain their values after power cycling, covering various data types including structures. Unfortunately, this feature simply fails to work on my workstation.

I’m also encountering a secondary defect: when creating new variables, I cannot select any structures or library function blocks via the graphical picker. I’m forced to either manually type the type names or directly edit the project source files, which creates a huge workflow bottleneck and is extremely troublesome.

What’s worse, I can’t change any mapp/AR versions in the project.it seems all clickable selection functions are malfunctioning on my end.
This same category of issues also occurs on my colleague’s workstation.

for sure @jianing.kang today is not your B&R lucky day…
On my side I tested permanent variables with X20CP3687X and no problem.

Could you call our Support in your area? Maybe you have to delete some cache/temp files/folder and rebuild them, they have all instructions.

Please update us when you’ll find the cause of the problem with AS 6.7 installed on your pc.
Ciao
Valerio

Honestly speaking, there are far too many obvious bugs ever since we switched to AS6. Fortunately, version 6.5 works pretty well.

I’m from the China region and will reach out to the support team.