Greetings,
I am encountering an issue following the migration of a B&R machine from Linux B&R 9 to Linux B&R 12.
I have reinstalled the Hypervisor using the identical configuration that previously functioned seamlessly under B&R 9. Under B&R 9, all systems operated correctly:
- The Hypervisor virtual network interface was present;
- Visualization was fully accessible;
- Chromium launched automatically at startup, displaying the HMI page hosted by the Runtime.
Since the transition to B&R 12, however:
- The Hypervisor virtual interface no longer appears in the Linux network interfaces (as verified via âip addr showâ);
- Only physical network interfaces are visible;
- The IP address previously used to access the visualization is no longer identifiable;
- Chromium no longer launches the HMI page automatically;
- It remains unclear whether the visualization is still hosted or accessible.
A peculiar observation: I can still communicate with the CPU via an IP address that does not correspond to any interface visible under Linux, which appears anomalous.
Regarding the Hypervisor:
- The ârth-virt.serviceâ fails to start properly;
- The device â/dev/rthBaseDrvâ is absent;
- During the installation of RTH components, I observed errors such as:
- âcould not insert âvnetDrvVirtâ: Invalid argumentâ;
- âcould not insert ârthBaseDrvVirtâ: Invalid argumentâ;
- Additionally, PCI-related messages concerning 32-bit BARs appear during boot.
I would appreciate clarification on the following points:
- Should the Hypervisor virtual interface be automatically recreated under B&R 12?
- Could the absence of this interface account for the loss of access to the visualization?
- How can one identify the actual IP address utilized by the Runtime if it does not appear in the Linux network interfaces?
- Is there a specific procedure for migrating or restoring the Hypervisor between B&R 9 and B&R 12?
Thank you for your assistance.