# Smaller array equal to Subarray of Larger array

**URL:** <https://community.br-automation.com/t/smaller-array-equal-to-subarray-of-larger-array/4930>\
**Category:** Programming\
**Tags:** automation-studio\
**Created:** [November 18, 2024, 12:49pm UTC](https://community.br-automation.com/t/smaller-array-equal-to-subarray-of-larger-array/4930 "2024-11-18T12:49:55Z")\
**Posts on this page:** 6\
**Page:** 1

<div class="post-metadata">

**Author:** ![adamkujawinski](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/adamkujawinski/32/4007_2.png) [@adamkujawinski](https://community.br-automation.com/u/adamkujawinski)\
**Post date:** [November 18, 2024, 12:49pm UTC](https://community.br-automation.com/t/smaller-array-equal-to-subarray-of-larger-array/4930/1 "2024-11-18T12:49:55Z")

</div>

I have a larger array example of x as type usint[0..99] which contains certain addresses I want to isolate.

It would be extremely convenient to do any one of the following as the array masking is varies

Option 1  
y as type usint[4..5]  
y := x // where y[4..5] = x[4..5]

Option 2  
y as type usint[0..1]  
y := x[4..5] // where y[0..1] = x[4..5]

Option 3  
y as type uint  
y := x[4..5] // where y = usint[2] to uint

is it correct that masking and Subarrays are not supported in Automation Studio? I’m trying to avoid multiple lines to take larger data sets. We have a series of parameters which range from one bit to 64 bytes and their address in an array vary depending on the machine used so being able to change a few enumerators would be quite an advantage.

---

<div class="post-metadata">

**Author:** ![tommi.piiparinen](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/tommi.piiparinen/32/2183_2.png) [@tommi.piiparinen](https://community.br-automation.com/u/tommi.piiparinen)\
**Post date:** [November 18, 2024, 1:16pm UTC](https://community.br-automation.com/t/smaller-array-equal-to-subarray-of-larger-array/4930/2 "2024-11-18T13:16:48Z")

</div>

Two suggestions for you depending on whether you want to copy the data, or just use a pointer to it. Both of them work with all of your Option variants.

Copy the data to a new variable. (Data in y is only updated when this line is executed, changing value in y does not affect x).

```auto
brsmemcpy(ADR(y), ADR(x[4]), SIZEOF(y));

```

Use pointers.

Define y as what you want as a “reference” and use the following line. (Data is updated in y as soon as it is updated in x. Changing values in y will also change it in x)

```auto
y ACCESS ADR(x[4]);

```

Example code below:

Variable definitions

 ![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/6/68c3d7c322a69368cb2c5d825fab9356e03e4c11.png)

Code:

```auto
PROGRAM _INIT
	// Preset example data
	FOR i := 0 TO 99 DO
		x[i] := i;
	END_FOR;
END_PROGRAM

PROGRAM _CYCLIC
	
	// Option by copying to new variable
	brsmemcpy(ADR(y), ADR(x[4]), SIZEOF(y));
	
	// Different options with pointers
	Option1 ACCESS ADR(x[4]);
	Option2 ACCESS ADR(x[4]);
	Option3 ACCESS ADR(x[4]);
	
END_PROGRAM

```

Values in Watch

 ![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/a/a26041e34bbef0b8f4993e960f9ff0a4c7a166ec.png)

---

<div class="post-metadata">

**Author:** ![adamkujawinski](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/adamkujawinski/32/4007_2.png) [@adamkujawinski](https://community.br-automation.com/u/adamkujawinski)\
**Post date:** [November 18, 2024, 2:41pm UTC](https://community.br-automation.com/t/smaller-array-equal-to-subarray-of-larger-array/4930/3 "2024-11-18T14:41:22Z")

</div>

Your solution works great, and was exactly what I was looking for in the original post.

That being said, I have now raised another concern.

After some “I swear I did that already”, my issue seems to have come from referencing within a structure.

 ![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/c/c2b10893c41da641085f8325b26641b3339fa275.png)

 ![image](https://europe1.discourse-cdn.com/brcommunity/original/2X/0/0d93b4cbdcbb2ce85eb37648e9321207217cb388.png)

```auto
//Works
y ACCESS ADR(x[4]);

// Does not work
z.y ACCESS ADR(x[4]);

```

just as an added bonus, referencing z does not work either.

Error 1392: Dynamic Variable required for Access

---

<div class="post-metadata">

**Author:** ![marcusbnr](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/marcusbnr/32/256_2.png) [@marcusbnr](https://community.br-automation.com/u/marcusbnr)\
**Post date:** [November 18, 2024, 3:40pm UTC](https://community.br-automation.com/t/smaller-array-equal-to-subarray-of-larger-array/4930/4 "2024-11-18T15:40:51Z")

</div>

Hi Adam,

Unfortunately, it is not possible to do this. You can’t include a dynamic variable as part of a structure (at least within IEC languages like Structured Text). The entire structure would have to be dynamic. Your options are:

1. Use a non-structure variable to reference a non-structure variable
2. Use a non-structure variable to reference a member of a structure variable
3. Use a structure variable to reference a structure variable

Something you could do is make the variable z.y a UDINT and store the address you want to reference:

> z.y = ADR(x[4])

However this isn’t a dynamic variable which means you’d then have to either pass this address into a function, or access it with another dynamic variable (residing outside of a structure).

---

<div class="post-metadata">

**Author:** ![adamkujawinski](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/adamkujawinski/32/4007_2.png) [@adamkujawinski](https://community.br-automation.com/u/adamkujawinski)\
**Post date:** [November 18, 2024, 3:49pm UTC](https://community.br-automation.com/t/smaller-array-equal-to-subarray-of-larger-array/4930/5 "2024-11-18T15:49:46Z")

</div>

> [@marcusbnr](#):
>
> You can’t include a dynamic variable as part of a structure (at least within IEC languages like Structured Text)
> 
> 1. Use a non-structure variable to reference a non-structure variable
> 2. Use a non-structure variable to reference a member of a structure variable
> 3. Use a structure variable to reference a structure variable

I did not achieve success when all of my variables were set to dynamic within the structure. So the third Option you suggested was tested and at the very least, I have not had any success. I decided to use a non-structured pointer to reference a structured variable as my solution.

---

<div class="post-metadata">

**Author:** ![marcusbnr](https://dub1.discourse-cdn.com/brcommunity/user_avatar/community.br-automation.com/marcusbnr/32/256_2.png) [@marcusbnr](https://community.br-automation.com/u/marcusbnr)\
**Post date:** [November 18, 2024, 4:16pm UTC](https://community.br-automation.com/t/smaller-array-equal-to-subarray-of-larger-array/4930/6 "2024-11-18T16:16:23Z")

</div>

Sorry if that was unclear. You can use a variable of a _structure type_ to reference another variable of the same structure type. You cannot reference anything with a structure _member_.

Glad you have a working solution though!