=====================================================================
I have reported the issue to our Support, I’ll update you once I have an update.
=====================================================================
on my PC at the moment I can configure your card only with AS 4.2.4.149 + 5ACPCI_XPNM_00 hw upgrade 1.2.0.2 + DTM 1.7.3.1
ensure nothing from Hilscher is still installed (check for “DTM” and “hilscher” in the apps)
delete the folder “SYCONNet” from C:\ProgramData
Delete the folder “Hilscher GmbH” from C:\Program Files (x86)
take a look at the Registry (“regedit”) if Hilscher got deleted within “Computer
HKEY_LOCAL_MACHINE\SOFTWARE\WOW6432Node\Hilscher GmbH”
→ “Device Library” and “DTMs” and “GenericSlaveDTM” should be gone
grant the user FULL Admin Rights
Reinstall latest DTM from our homepage
→ This time the registry should contain Device library and DTMs:
If above visible entries are NOT here the installation failed (please note that the amount of “kryptic”
entries can vary but at least a few must be available)
Start AS and the errors should be gone (probably you have to delete the NetX card and reenter it
again)
Hi @Erkan_Birol ,
I did a search with AI and I don’t think the message is related to Automation Studio:
“Insert the ‘CX Common Tools’ disk” is an error message that typically appears when installing or updating OMRON CX-One, a comprehensive software suite used for programming and configuring OMRON PLCs (Programmable Logic Controllers) and industrial automation components.
This message means the installer cannot locate necessary shared components (like CX-Integrator, CX-Designer, or CX-Protocol) that are part of the CX-One package.
What This Means & Why It Happens
Missing Installation Media: The installer requires the original DVD-ROM or ISO file to be inserted/mounted to pull additional files.
Interrupted Installation: The installation process was interrupted, or the installer files were moved after the installation started.
Virtual Drive Issue: If installing from an ISO image, the virtual drive may have been unmounted by the system.
How to Fix It
Insert/Mount the Media: If you are using a DVD, re-insert it. If you are installing from downloaded files, ensure the CX-One ISO image is still mounted as a virtual drive.
Point to the File Location: If the error provides a file path, browse to that location within the setup folder (usually labeled “Common” or “CX-Common”).
Copy Setup Files Locally: Copy the entire contents of the disk or ISO file to a local folder on your computer (e.g., C:\OmronSetup), and run the setup.exe from there.
Run as Administrator: Right-click the setup.exe file and select “Run as administrator” to ensure the installer has permission to access all files.
Clean Installation: If the error persists, you may need to use a cleaner tool (like CX-Remover) to remove the broken installation and start again.
===============================
Is it possible that you have uninstalled a package related to OMRON?
I hope it helps
Ciao
Valerio