In the AS6 Help, the script below for connecting MpDatabase to a database cannot be downloaded (clicking on it does nothing), whereas it can be downloaded in AS4. Could you please help me figure out how to resolve this, or simply provide me with the script?
Sorry for responding to an already solved topic, but…
Please be informed that the script you can “download” from the help is obsolete (starting with mapp Services 6.8.0) and should not be used for new developments anymore. As the help states, this version of the connector/proxy cannot fulfill modern security expectations and is provided mainly for compatibility with older mapp Services versions. Going forward, mapp Services will not maintain and/or update this version of the script.
The “Samples” folder of AS is usually (with a default installation of AS6) located under C:\Program Files (x86)\BRAutomation\AS6\Samples, and (if you have installed mapp Services 6.8.0) should contain a file named mappDatabaseProxy-6.8.0.zip. This script will be the version going forward, and will be the only one maintained by mapp Services.
Why is this new version of the script not directly available in the help?
As you have already noticed, it is not possible to “download” the script from the online help, but only when you use the locally installed “offline-help”. This is due to limitations outside the control of mapp Services, in that the help does not actually download anything, but simply copies the script from it’s own local directory to a location you provide. Currently, there is no possibility to provide an actual “download” for the script. That, and the fact the help is not versioned, but overwrites older versions, have been the main reasons we decided to put the current script into the Samples folder of AS, which is always available, allows us to version the script, and is independent of the help.