Unable to Copy IP Parameters from Project to a New X20CP0484 Controller – “No SNMP Variables Currently Available”

Hello everyone,

I am facing an issue while trying to copy the IP address from my Automation Studio project to a new X20CP0484 controller

Whenever I try to copy the IP parameters from the project, the following error appears:
System.InvalidOperationException: No SNMP variables currently available

Details:

  • Controller: X20CP0484

  • SNMP: Activated

  • Error: “No SNMP variables currently available.”

  • Additional observation: The same controller and project work correctly on another PC with the same configurations. The issue occurs only on one PC.

Troubleshooting already performed:

  • Verified that SNMP is activated.

  • Tried running Automation Studio as administrator.

  • Tested with the same controller and project on another PC, where the operation works correctly.

Despite these attempts, the issue persists on the affected PC.

Has anyone encountered this issue before? Could it be related to the Automation Studio installation, SNMP configuration, or any missing component or Windows dependency?

Any suggestions or guidance on how to resolve this issue would be greatly appreciated.

Hello,

Automation Studio uses the PVI package for SNMP protocol.

PVI uses a 3rd party DLL derived from Wireshark project for that.

So I would try to reinstall PVI.

Which PVI - Version is installed ?

see Setting IP address on X20CP3684 - Ask Questions / B&R Software & Runtime - B&R Community

and Finding/Browsing PLC in Online Settings not possible under Windows 11 - Ask Questions / B&R Software & Runtime - B&R Community

I had one issue with snmp and pvi 6.7.1:

I downgraded to 6.7.0 and no more issue. Feedback from R&D in that time PVI 6.7.1.13 has the fix.

Ciao
Valerio