X20PS9600 LEDs and RS485 frame error

I am using X20CP0484-1 + X20BB53 + X20PS9600 with MODBUS/RTU com. The communication is operarating, but the leds on X20PS9600 not working.

The terminating resistor in X20BB53 is ON and I can see it also in status bit from X20PS9600, but the LED T is off.

The S LED is also off even if communication working.

And for RS485 I have frame error. It’s work, but I don’t know why. I think, that’s from switching from TX to RX mode, because when I change TEMTS, the timing of “restlessness on the line” moved in timeline (it’s have about 4us). I wouldn’t worry about it, but I did encounter error 20262 at one point, when the slave returned “illegall address”. This frame error was here even if I turn off the slave.

This is my settings for RS485: ‘/PHY=RS485 /PA=E /DB=8 /SB=1 /BD=19200 /TEMTS=1’

Hello Jan,

Please check that PS9600 you have is actually PS9600 and not PS9602, check logger and sdm. just in case also try switch the resistor switch in case there are some contact problem.

Regarding the frame issue, please can you give us some more information?, I assume you using it master (PLC as master) and reading register from a slave, how are doing it ? using DV_frame or DRV_mbus? there can also be disturbances that generate the error

Yes, it is PS9600. In log or SDM is nothing weird. I just have only CPU on table so the IO modules not present.

I also test it on different HW and it didn’t ON the LED for COM or Term. Also test ON/OFF switch.

For the frame I use the DRV_mbus and like master. I think, that’s can be solved, because I don’t have problem with it. Just for info.
Next picture is from /TEMTS=0 - just move in time. Maybe it’s broblem, that I test it on desk and some wiring/measuring problem.

Hi @NovotnyJ what is status of your issue? have you solved it or contacted support in mean time? thanks for update

I am waiting for response from local support.

Understood. I tagged question support-ticket and am asking you to update us with a solution or findings from support. Have a nice weekend.