IO Link V_Pd_OutrunMode

Dear Mateo,

I did not encounter the error that you are talking about, the only thing that happened to me was that the lights stopped responding.

I have been thinking about it but sadly I do not know how to solve your issue.

All the best,

Walid el Oufi

Dear Noah,

B&R sent me the file I shared on September 17th. They only told me that the ASFltGen2 library was the issue and that they used another library.

With the other library it worked as it should have when they tested it.

Sadly the project The LED strip was for is on hold, so I did not dive into the library to figure out what they changed yet.

Kind Regards,

Walid el Oufi

Dear Noah,
I have the very same problem then you.
I can 24 times send a command, then the ligth stucks and plc crashes and tells me, the io link module is offline.
If it is really caused by the library, where to get the updated version from?
Thanks and regards
Lucas

Hi Lucas.

It was not the library that was causing the issue I was having but rather an internal read buffer that overflowed and caused the card to run into an error state. This is fixed by “reading” an acknowledgment from the write cycle of the card to clear that buffer. Here is the code that fixed it for our system. Of course you will need to update the variables to your own but the concept is all the same.

I have two write sequences as I am writing to two different lights. The error happens every 24 write cycles to the combined number of channels that is being used. i.e. 2 channels means 12 total write cycles (2 to each channel). You can copy and reuse the write cycles for the channel 3 or 4 as well.

FLT_WRITE1:			(* send data *)
			
			(* set Sender.size of frame *)
			Sender.FLT_write.enable := TRUE;
			Sender.FLT_write.bufLen := SIZEOF(Sender.send_data);
			Sender.FLT_write.pBuf 		:= ADR(Sender.send_data);(* enable the FUB *)
			Sender.FLT_write();									    (* run FUB *)
			
			IF Sender.FLT_write.status = ERR_OK THEN
				Sender.step := FLT_WAIT_ECHO1;			        (* if data was written, goto start *)
			ELSIF Sender.FLT_write.status <> 65535 THEN
				Sender.step := FLT_ERROR;						    (* if something goes wrong -> ERROR *)
			END_IF	
			
		FLT_WAIT_ECHO1:		(* wait for the echo from the other side *)
			Sender.FLT_read.enable  := TRUE;						(* enable the FUB *)
			Sender.FLT_read.pBuf	:= ADR(Sender.recv_data);		(* announce recv buffer to the FUB *)
			Sender.FLT_read.bufLen  := SIZEOF(Sender.recv_data);	(* set the recv buffer length *)
			Sender.FLT_read();										(* run FUB - acknowledge recveived data *)
				
			Sender.FLT_write.enable    := TRUE;						(* enable the FUB *)
			Sender.FLT_write.pBuf   := ADR(Sender.send_data);	  		(* announce frame data to the FUB *)
			Sender.FLT_write.readSequ := Sender.FLT_read.readSequ;	(* acknowledge the recveived data to the HW-Module *)	
			Sender.FLT_write.bufLen	  :=  0;							(* only acknowledging - no data to send *)
			Sender.FLT_write();										(* run FUB - acknowledge recveived data *)
			//Sender.step := FLT_READY;
			
			IF 	Sender.FLT_read.status = ERR_OK	THEN
				;						// no data received run again 
			ELSIF	Sender.FLT_read.status = fltERR_FRAME_FINISHED THEN
				Sender.step := FLT_CHECK_ECHO1;						//(* frame was completed in the recv buffer 
			ELSIF Sender.FLT_read.status = ERR_FUB_BUSY THEN
				;													//(* some frame was insert in the recv buffer, but the frame is not finished
			ELSE 			
				Sender.step := FLT_ERROR;	
			END_IF
			
		FLT_CHECK_ECHO1:		(* check the received echo *)
			IF (Sender.send_data[0] = Sender.recv_data[0]) AND
				(Sender.send_data[1] = Sender.recv_data[1]) AND
				((Sender.send_data[2] AND 2#00000111) = (Sender.recv_data[2] AND 2#00000111)) AND
				(Sender.send_data[2].7 = Sender.recv_data[2].7) THEN
				Sender.step := FLT_WRITE2;					(* if the echo match -> reset *)
				brsmemcpy(ADR(Sender.command.ioLinkReceive[0]), ADR(Sender.recv_data[3]), SIZEOF(Sender.command.ioLinkReceive[0]));
				Sender.command.start := FALSE;
			ELSE
				//	Sender.step := FLT_ERROR;					(* if the echo doesnt match -> ERROR *)
			END_IF
			
		FLT_WRITE2:			
			Sender.send_data[0] := Sender.command.Channel2;				
			Sender.FLT_write.enable := TRUE;
			Sender.FLT_write.bufLen := SIZEOF(Sender.send_data);
			Sender.FLT_write.pBuf 		:= ADR(Sender.send_data);
			Sender.FLT_write();									    
			

			
			IF Sender.FLT_write.status = ERR_OK THEN
				Sender.step := FLT_WAIT_ECHO2;			        
			ELSIF Sender.FLT_write.status <> 65535 THEN
				Sender.step := FLT_ERROR;						    
			END_IF
			
		FLT_WAIT_ECHO2:		
			Sender.FLT_read.enable  := TRUE;						
			Sender.FLT_read.pBuf	:= ADR(Sender.recv_data);		
			Sender.FLT_read.bufLen  := SIZEOF(Sender.recv_data);	
			Sender.FLT_read();										
				
			Sender.FLT_write.enable    := TRUE;						
			Sender.FLT_write.pBuf   := ADR(Sender.send_data);	  	
			Sender.FLT_write.readSequ := Sender.FLT_read.readSequ;		
			Sender.FLT_write.bufLen	  :=  0;						
			Sender.FLT_write();									
			//Sender.step := FLT_READY;
			
			IF 	Sender.FLT_read.status = ERR_OK	THEN
				;						// no data received run again 
			ELSIF	Sender.FLT_read.status = fltERR_FRAME_FINISHED THEN
				Sender.step := FLT_CHECK_ECHO2;						//(* frame was completed in the recv buffer 
			ELSIF Sender.FLT_read.status = ERR_FUB_BUSY THEN
				;													//(* some frame was insert in the recv buffer, but the frame is not finished
			ELSE 			
				Sender.step := FLT_ERROR;	
			END_IF
			
		FLT_CHECK_ECHO2:		
			IF (Sender.send_data[0] = Sender.recv_data[0]) AND
				(Sender.send_data[1] = Sender.recv_data[1]) AND
				((Sender.send_data[2] AND 2#00000111) = (Sender.recv_data[2] AND 2#00000111)) AND
				(Sender.send_data[2].7 = Sender.recv_data[2].7) THEN
				Sender.step := FLT_READY;					
				brsmemcpy(ADR(Sender.command.ioLinkReceive[0]), ADR(Sender.recv_data[3]), SIZEOF(Sender.command.ioLinkReceive[0]));
				Sender.command.start := FALSE;
			ELSE
				//	Sender.step := FLT_ERROR;					
			END_IF

I hope this helps!

Dear Noah,
thanks for sharing your code.
I have tried the B&R example posted here earlier DS438A_example.zip.
Some modifications and working well.
Now I have one LED stripe for testing, later 5 pieces…
I have shifted the tasks for comm libraries from TK#1 2ms to TK#8 and is still working.
Best regards
Lucas