Hi @Torsten_K ,
thanks to @Samuel I found the libary now ![]()
I canāt check the source or functionality since the origin project on the library base is an AS2.5.x project, and I donāt have a suitable installation available right now.
But from what I see in the documentation (pls. see screenshot below), it doesnāt seems that a functionality to āserialize the data directly into a stringā is implemented.
So I think, the best approach to follow could be:
- check if the recipe file data size is suitable to be stored inside a string variable (like described by @michael.bertsch )
- if yes, you could try to
- 1.) use the dat_mod library as intended by creating a file export
- 2.) use FileIO functions āFileOpen, FileRead, FileCloseā to read the exported file content into the string variable
- 3.) delete the export file via dat_mod functions to keep the database up-to-date
Last but not least hereās a āsmall life hackā about string sizes, that I used here and there:
if you declare an array of strings, the whole array size is on block inside the memory.
So if you memcpy() string data to the first string element, where data is longer then one array element size, because of the overflow of the first string element the rest of the string data will be copied into the 2nd element, and so onā¦
⦠of course this is no ānice programmingā, and you still have to take care that the data size is not greater then the complete array memory to avoid page paults or other issues.
But sometimes using such overflow can be even useful: for example I used string arrays to make my whole string data available via Automation Studio Watch.
As the size of string data in the watch is limited to 80 characters, using a string array of element size 80 and memcpying the longer string to this string array makes it possible to watch more string content ![]()
Best regards!