APROL R 4.4-00 Industrial Control System launched

The new APROL release is based on the new SUSE Linux Enterprise Server 15, which means that important APROL components have been updated to the latest versions, including Linux kernel 5.14, OpenSSL 3.0, MariaDB 10.6, PHP 8 and PostgreSQL 14.

This is an important basis for ensuring IT security. The operating system is hardened for critical applications and fulfils the security requirements of networked production systems.

5 Likes

Martin, thank you for this information.
In this APROL Video Guide: Release information APROL R4.4-00 you can find additional information

Note:
The contents are only visible when logged in . You can log in using the access data for the B&R website . B&R customers can obtain their access data from their B&R sales representative or use our Contact form.

1 Like