If I use directly DINT_TO_REAL I will get value like the picture below:
But Customer want to get the value of IEEE 754 float:
3.6440908908843994
![]()
Do we have such functions?
Hi,
REAL is already IEEE 754, so no need to convert it.
if you need to see the bit representation then just memcpy REAL to UDINT (or DINT or DWORD).
Hi,
if I understand this correctly the REAL value comes split up in two 2-byte values (gVar1, gVar2), maybe over a network.
These two values are combined into one 4-byte value (gDWORD) and should be shown as a REAL again.
Create a dynamic REAL vaiable (e.g. dREAL)

In the code use the “ACCESS” operator:
dREAL ACCESS ADR(gDWORD);
This is what we get

Thanks both are good ideas for this issue.