I recently rediscovered that it’s possible to create custom file type filters for the Find in Files dialog. This can be done by editing the “FileFilter.cfg” configuration file found in the Automation Studio install directory (e.g., C:\Program Files (x86)\BRAutomation\AS6\AS\ApplicationSettings for Automation Studio 6).
I added a new element to the 6th slot containing the file types I often search:
Disclaimer: Make sure to back this file up before you edit it! This is a workaround rather than an intended feature, so I’m sure it’s possible to break something.
If you only need a quick custom filter you can also just enter your filter criteria into the selection field.
It will remain there as option until overwritten with something else.
You learn something new every day! Interestingly, when I create the filter that way, it doesn’t modify the config file.
I did confirm that, via the config file, I’m able to create multiple custom filters that are saved between AS restarts. Your way seems a little easier but at least I have a solution for that if that’s ever needed.
Do you know if this feature is also available in AS6.5.3.11?
The list doesn’t seem to update for me when I type something in manually.
The “File types” entry remains there the next time I open the dialog, but the entry I typed isn’t added to the selection list.
In my registry, I can only find the FindInFilesData entry for AS4.12.
Hi Simon,
I’m running AS 6.7.1.4 SP and just used “File types” the other day. I went back and unfortunately the filter is not saved which is very unfortunate