Spettacolo, this is the future! no context only couple of screenshots.
Hello,
to get little bit more into context…
The Pictures show you are using MappView.
The Keyboard Definitions belong to VC4.
- These are two different Systems, which one do you want to use ?
- Is this a Project which resulted by upgrading/changing an old Project?
- The USB Interface on the 2ten Picture is connected to the Terminal (Linux) System not to the Automation Runtime. Why do you want to add there a Keyboard Definition?
Long story short … if MappView is used delete the Keyboard Mapping Files.
Greetings
Michael
If the topic does not have at least minimum quality, you can all use the flag and report it to the moderation team. Use the “Other” option and add info that it has bad quality..
@Progics005 Your topic was unlisted until you provide at least minimum technical information like what you would like to achieve, what you have done, what version of AS are you using,…etc, etc and printscreens. To provide only pictures is usually not enough.
How to use a USB keyboard to trigger actions and change pages on a 4PPC50.0702-10B using vc4
-
When I connect the keyboard, I only get an arrow on the screen. Keys do not trigger any actions.
-
In the Visu editor I see this message: “no visualization object mapped to the file VC\USB-Keyboard.dis”. I cannot select the keyboard or a key mapping filethese are my problems
-
What are the exact steps to configure a USB keyboard for VC4 on this panel?
-
How do I link the USB-Keyboard
.disfile to my visualization object, so the “no visualization object mapped” message goes away? -
Where do I assign keys to actions, such as the key mapping (
.kmp) file, key levels, or the “Key” setting on a button? -
Is a special configuration needed for page changes by keyboard, or for moving focus between buttons using the arrow keys and Tab?
can u help me to solve this
topic listed back for global audience.
hi @Progics005 I wound this old topic, can you update us with your final solution?
“I didn’t get any solution.