OPC UA Reverse Connect option available in is B&R.
If it is there, please share the details
OPC UA Reverse Connect option available in is B&R.
If it is there, please share the details
OPC UA Reverse Connect in B&R means that the OPC UA server (e.g., the PLC) initiates the connection to the OPC UA client, instead of the client connecting to the server. Is this what you are looking for? As far as I know, B&R OPC UA server can reestablish connection with the client if the connection is lost, but I’m not aware of functionality that allows the OPC UA server to initiate connection.
Yes exactly
Reverse Connect function of OPC UA to establish a backward communication connection
from the server to the client
Hm, as I mentioned in the previous comment, reestablishing connection is available. Establishing connection from OPCUA server to OPCUA client is not, as far as I know. This is a possible product request and this must be asked using your local country sales representative or maybe support contact.
Thanks for your valuable support.
can you please share related document link it will help me lot.
we will contact our local B&R supplier.