Redundant Runtime PC's Synchronising to B&R X20 Controller setup as NTP Server

Hi,

We currently have a redundant pair of X20 controllers configured as NTP time server, using their internal clocks as the time source and with the stratum level set to 3.

Our redundant APROL runtime PCs are configured as NTP clients to these controllers. However, we’re experiencing significant delays in time synchronization — in some cases, it can take several hours for the clients to update. During the synchronization process, we’ve also observed instances where the system clock on the APROL runtime appears to freeze, which in turn leads to further issues within the system.

Has anyone encountered similar behaviour with this setup? I’d appreciate any guidance or recommendations on how to troubleshoot and fine-tune the NTP client configuration on the APROL side to achieve more reliable and timely synchronization.

Best regards,
Dale

hi,Dale
I remember it seems that the configuration of NTP can be manually configured in YAST, but I really can’t remember clearly. Maybe you can check it out.

Hi,

Thanks for your response. I’m a bit unclear about which NTP service the APROL system actually uses — does it rely on standard Linux services like chronyd or ntpd, or does it have its own built-in mechanism for handling time synchronization?

Any clarification would be appreciated.

There is an ntpd service.

You can also open YaST, click on ntp inside, and it should be possible to configure the time synchronization.

But to be honest, I really can’t remember clearly. Perhaps you could take a screenshot?

service ntpd status


Or u can ajust NTP configuration in YaST

Of course, by default, NTP refuses synchronization if the time difference exceeds 1000s. You can add parameters to adjust this limit, such as the straightforward tinker panic 0
Or, after detecting that NTP has stopped, directly use ntpdate to force synchronization and then start ntp again. If you can accept the risk of time jumps or time repetitions.

Good Morning,

As far as I’m concerned the only configuration we have implemented for the NTP Client is in APROL config as shown below. Our NTP server is 172.16.1.20.

This is the configuration setup we currently have for the Controller acting as the NTP server. The controllers configured as NTP clients synchronize relatively quickly and without issue. However, we are experiencing delays with the redundant runtime PCs and operator station, which take significantly longer to synchronize.

I haven’t made any changes to YAST in any of the redundant PC’s or operator stations. I wasn’t sure if APROL dealt with this.

Regards,
Dale Webb

Good Morning,

Noticed some improvement in the Synchronisation speed, now looks to be less than 10 minutes which is much better, So thank you for that.

However this only seems to work when going forward in time, when going back in time the APROL system time seems to freeze. Once frozen the only way to restart the APROL time is by stopping and starting Runtimes using Start manager, which is not ideal.

I feel like this may be another issue that I may have to raise as a support ticket.

Regards,
Dale Webb

You can check the NTP status of your APROL server in command line with “ntpq -p”.

image

No additional configuration in Yast should be necessary for NTP configuration if you have configured NTP in AprolConfig.

For redundant Runtime Servers it is recommended that they are configured to each other (additionally to another time source) . Means the Master has configured the Client Server as NTP Server and vice versa.

Hi,

Thanks for the response. I have updated the configuration and the two runtime servers are now pointing at each other as well as the NTP server. Unfortunately still seeing the APROL system time freezing when trying to go backwards in time.

Kind Regards,
Dale Webb

Hi @Dale_Webb , can you update us on what the final solution for your issue was?

Hi @Dale_Webb , what is your status of your topic? Can you update us and mark question that has helped you the most?

Hi,

This configuration wasn’t suitable for a Marine application where we required all System time across all redundant PC’s and Controllers to be changed instantly from the GUI.

Using a controller as an NTP server for a Redundant PC setup led to Crashes and unstable system. It also could take a day before the time would change and often crashed the runtime.

Our solution to the problem was to instead use the redundant runtime PC’s as the NTP server. Set the time on all PC’s using a SSH command followed by a full system reboot.

Thanks.

Thanks for sharing your findings.