Hi BnR Community,
I’m looking for a way to set the max and min limits for numeric input using a variable instead of hardcoding the values. Is there a method to bind these limits dynamically?
I’d appreciate any guidance. Thank you!
Hello,
the widget does not provide dynamical settings for Max and Min.
If you need this, you have to use the Unitsystem from the OPC UA server => B&R Online Help
You can set different limits for different roles and also use other OPC UA variables for the limits. See B&R Online Help
For inputs you can also decide on the OPC UA server what action to perform when a limit is violated.
BR
Fabian
2 Likes