Onlinechart widget: zoom with EU limits

I use Onlinechart widget. I need to change chart limits in real time (I tried autozoom, but it seems it doesn’t correspond my demands). So I need to autozoom chart myself with signal’s EU. I tried to bind two PV for high and low EU limit of charts value, but it has no affection on chart.
How can I change Onlinechart’s high and low limits “on the fly”?

Hi Andrey!

The min and max value of OnlineChart widget are not bindables, so I you cannot change those parameters with the values you want.

OnlineChartGraph:

However, you can use the autoscale parameters to adapt automatically the chart to minimum and maximum values. Just define this parameter to “true” in OnlineChart widget.

OnlineChart:

I think you did not bind your value as a node to Online Chart. Then EURange is taken as a limit, not limits from widget itself. Check my example.


Thank you, Jaroslav! It is worked out.