The number of graphs in OnlineChartHDA

Hello, community members.
I am looking for a way to increase the number of graphs in OnlineChartHDA from a maximum of 10 to 48. Is it not possible to use more than 10 graphs in OnlineChartHDA?

Thank you.

Hello @frogman

the number of graphs and y axis is limited to 10 by the system. I have no information to increase that number or that this will be increased in future.

Depending on the screen more than 10 graphs might be confusing anyway.
Despite the fact that more graphs mean the need of more performance for the client, 10 is somewhat the sweetspot for most target.

To make this a bit dynamical you could use listbindings to select the displayable signal for each graph.

BR Fabian