Hi Community!
Does anyone have a good example for driving a motor with ramp mode?
I want to run the motor with as little delay as possible between two positions after getting a trigger.
Thanks in advance
Hi Community!
Does anyone have a good example for driving a motor with ramp mode?
I want to run the motor with as little delay as possible between two positions after getting a trigger.
Thanks in advance
The smallest MPGen cycle with Ramp is 5msec. With Module configuration 1
Δs / Δt you can reach smalller cycles, depending on CPU load, X2X,PLK, SDC cycle time settings.
Thank you for the hint - What I read from your reply is that using SDC mode (with MotorStep ds/dt and creating the ramp yourself after reading the trigger) will result in a faster reaction, because the module has an internal “delay” of 5ms for the internal profile generator, when used in ramp mode?
The Target reached (MpGenStatus01) will also be updated every 5msec, and this information has to reach the cpu. With deltaS/deltaT this profile information is calculated faster and in the cpu.
Hi @patricthysell ,
It looks like you got some good suggestions from other community members, and it has been a couple of weeks since the last activity on this post. Can you please mark the reply that helped you the most as the solution? Or if you still have open questions on this topic, can you please provide an update?
Jaroslav