Where to download ACOPOS Inverter P66 hw upgrade V1.5.1?

Automation studio 4 open a project show up below infomation.How to find and download that module runtime application?
Required version ‘1.5.1’ for hardware module ‘FBE.0100006C_8I66XXXXXXX’ is not installed currently. Please install the corresponding upgrade

What happens if you click on “Download Required Version(s)”?
As written in your screenshot, by doing so you should be able to install the firmware the upgrade then.

It will be can not find out the same P66 modle and 1.5.1 version in the list.

I think the project you are using is using the .xdd file for P66.

This is not the official way we support our devices.
To get this file please get in contact with product management (josef.stoellinger@br-automation.com)

Thanks.I think this inverter need to replace a new model like P86.

No it’s not a old model. Just just have to switch to the official hardware upgrade - which you can download in Automation Studio or from our homepage. You are using the fieldbus device description file in your project and not the official P66 upgrade.

This would be the link to the offical upgrade:
https://www.br-automation.com/de/downloads/?tx_brcdn_downloadlist[action]=download&tx_brcdn_downloadlist[controller]=Download&tx_brcdn_downloadlist[id]=DWL%40DWL10000746148%4000&tx_brcdn_downloadlist[lang]=*&cHash=1914174a61083680ed826afe12f3da03

PS: P86 is not newer than P66, P86 has more performance and features. The newest generation (Px7) would be a P77 drive.

Thank you Thomas so much. Don’t know why the AS 4.2 version can not show the 3rd device like your.

Could you export your devices and share to me?