I’ve been testing out AS6, and I noticed an issue with mappCockpit. Its not showing the axes I have configured in my project.
In my ‘component overview’ screen, where i expect to see the axis references, its blank.
Just me?
Hi,
I’m not sure why it isn’t working at your side.
In my test project (it’s the mappView Highlight project plus one axis, ArSim) it looks good.
The change from AS4 / mappCockpit5 to AR6 / mappCockpit6 is, that you even have to be logged in with a user having at least read access to see anything.
Before login, I also can’t see any components:
After login, I see all the components:
The user I’ve used has the roles “Everyone” and “BR_Engineer” (for write access):

For preparation to use mappCockpit, I more or less followed this guide from the help.
Best regards!
Hello bjacot:
Another thing necessay for the cockpit to work for me was to to configure the BR_Engineer as an authorized user role, for this in the UaCsConfig.uacfg file:

Open the advanced configuration

And In the authorization add the BR_Engineer role:
After adding this, I was able to log in and have all the components.
I assume that since @alexander.hefner used the mappView Highlight, chances are that those configuration are already established.
Hope it works for you.
you’re completely right, thanks for this hint! ![]()
My project wasn’t setup from scratch, so this setting was already included and I forgot to mention it.
As Automation Studio 6 follows the Security-by-Default approach, if starting from “new project”, all the neccessary and / or wanted settings have to be done by the user on purpose.
great - that fixed my issue.
Thanks.
Hello
is possible like in AS4, have the read only access by default in cockpit?
So if we do not login, at least we can access data in read only mode
Many thanks
Marco Sartori
Hi,
I don’t think that it’ll be possible exactly like in AS4.
I’m not a motion expert, therefore I’m not using mappCockpit very often and so I’m also not 100% sure:
but I think to know, that mappCockpit will support the “anonymous token login” if configured inside the project like described here for mappView.
Not sure when it will be available (mappCockpit 6.3 ?), and also I’m not sure if that will meet your requirements.
If you’re asking as a developer, maybe it could make developing life a bit easier.
But in my opinion the most important topic to meet todays and future cyber security requirements is, that such a functionality should / must never be used in productive machines.
Have a nice evening, best regards!