B&R PLC and HMI development checklist/pre-requisite

Hello Experts,
I recently started working on automation studio and want to have a pre-requisite OR checklist that i can go through OR follow during PLC and HMI development on B&R software platform. It can be related to below things:

  1. Software installation
  2. Hardware(I/O) configuration
  3. Program development/testing
  4. Hardware testing.

Where i can find these details?
It will very helpful If anybody share in this community. Thanks in advance!

Hello Suraj,

I hope the following meets your expectations:

  1. Software installation
    The IDE / Automation Studio can be downloaded from the B&R homepage:
    Downloads | B&R Industrial Automation

There is a Help inside the Setup and on the B&R homepage:

B&R Online Help

There is a chapter on SW installation.

  1. Hardware(I/O) configuration

There is also a chapter “Getting Started”.
Gettig Started are available for the first Automation Studio project, for HMI, for HW Configuration …

  1. Program development/testing

There is also a chapter "Diagnostics and Service. If simple tests are sufficient then you can work with the diagnostic tool Monitor

  1. Hardware testing.
    If simple tests are sufficient then you can work with the diagnostic tool Monitor.

I can also recommend the B&R training courses for beginners. They also provide training modules for this.

Best regards Stefan

Thanks for the information!!