Can not connect to an SFTP Server with X20 Edge Controller, because firewall is blocking Psiphon

Hello, I found out that the firewall was falsely classifying the SFTP connection as Psiphon traffic.

With some help from AI, and by enabling verbose SSH logging and testing one parameter at a time, I found that the default OpenSSH handshake included the MAC algorithm hmac-sha2-256-etm@openssh.com, which triggered the firewall.

Excluding that single MAC from the SSH negotiation allowed me to connect without any other changes.

1 Like