Hi
I am using automation studio 6 and trying to add IEC 61131-3 functions library in my program. But the IEC Libraries appear in Object catalog are IEC check functions Library, and IEC Library. when i add IEC Library, it has nothing inside. I mean typ, var, and fun files are basically empty. please guide how can i get those functions.
IEC 61131-3 functions
Regards
Most of the IEC functions are included in the standard library.

The convert functions are included in the AsIecCon library.
Thank you for the reply it worked for the thing i was working before but to convert bool array to string i need AslecCon library but when i click it to add, it does not add in my program.
The AsIecCon is automatically added to the project, when creating a project.
I assume it is already in the project.