I am using meteorix servo drive as canopen slave in B&R automation studio and canopen Master X20IF2772 over controller x20cp3684. Also my purpose it to read/write TPDO and RPDO. I have used ascanopen Library and used sample program 2 for my reference to write a code. I have no errors in the code, but after transferring I am not getting any output. What could be the issue? Or I have to use some different method to read/write PDOS?
Also I am trying to simulate this drive, but I don’t have any hardware for this.
Thank you for your help.
Since you are simulating the drive, how are you checking for output? The first thing I recommend trying is forcing outputs (bypassing any control logic) to make sure that you are sending something with data rather than just zeros. Then, you can use a CAN sniffer tool/program (one example is PCAN. but there are others) to see what data the device is actually sending.
It’s hard to tell from just this post what the problem is. If you’re getting any error information (i.e. on function blocks or in the Logger) those would also help us diagnose.
I have written logic with variables and as per my code I am getting output but there is no can communication established . and I wan to get output over canopen protocol. i will try using PCAN or similar software as recommended by you. I just wanted to know is there any way to simulate canopen drive without hardware and without external canopen simulator.
Thank you @marcusbnr.
Sorry for the late response. The only drive simulation built into Automation Studio is for B&R servo drives, since B&R knows the properties of their drives and can simulate their behavior. If you wanted to simulate the process of a third-party drive, you could write a program that acts as the drive and responds to inputs by setting outputs. However, this wouldn’t use any of the CANopen data. If you wanted to use CANopen as part of your simulation (meaning you’re physically sending outputs and waiting for inputs to come back over the network), you’d need some sort of external device handling that simulation.
Let me know if that makes sense and keep us updated if you find a solution!
Hi @samikshaunhale21, what is status of your topic can you update us and close this topic?
closed due to inactivity of author. @samikshaunhale21 feel free to reopen if need it or you have new findings ![]()