Has anyone programmed a library to handle CANopen devices on a simple CAN interface? E.g. the X20CS2770 doesn’t have CANopen, and handling multi part sdo reads etc. manually is very inconvenient. But since everything is described in the CANopen spec, it should be possible to have a little wrapper lib to make life easier?! Anyone has something like it? Would be highly appreciated (and save me some work…)! ![]()
i will send you a Lib.
example project created with Automation Studio 4.7
CanOpMa_47.zip (162.2 KB)
CoMaDevice_en.pdf (73.4 KB)
Hi,
I am testing this library between two X20CS1070 cards but can’t make it work.
Can this library be used only for master-slave communication type or can also be used for direct data exchange between nodes?
Hello Andrius,
this library represents a CanOpen Master. In order to be able to establish communication between two X20CS1070 via CanOpen, a CanOpen slave is required on the second controller. This library does not offer this function.
Regards
Stephan
hello,
Did you try to use the CAN_lib library?
wit regards
sven
Hello Stephan,
Can we use above library CoMaDevice for preconfigured Salve Device by keeping enable input pSlave.Device.enable => FALSE, So that We can use Only PDO Read & write communication without Activating SDO, As we have preconfigured Slave Device
works great
thank you Stephan
Hello,
you can simply delete the data object from the software configuration. Then the slave starts with its preset values.
Regards
Stephan
Thank you for your feedback
Regards
Stephan
Hello Sven,
yes i use can_lib!
Regards
Stephan
Hi Stephan
I was using your wraper lib on top of a CAN interface to communicate with a slave. Your wrapper works and the description pdf looks ok but does not cover all. I am beginner and find it a bit hard to understand all- I would like to know if there is a decsription of how to send NMT command or just send a PDO (ID = 000 Data = 01 03 ( to slave 3)) to wake up the slave?
Thanks
Hello,
the function automatically sends an NMT protocol to start all slaves. If the slave fails during operation, the CanOpenMaster function sends a start to the CAN slave again.
Regards
Stephan
Hi Stephan
I used the wrapper lib on X20CS2770. I also have X20IF1043 CANOpen Slave. Will this slave be also started with the NMT protocl which your function sends? It seems it is not starting. Only a PDO (ID = 000 Data = 01 03 ) send via CAN sniffer starts it.
Regards
Matt
Hello Matt,
yes the X20IF1043-1 must also start with an NMT command identifier 0. According to your data the X20IF1043 must have the node number 3.
Gruß
Stephan
I changed the Node to 3 . But it is not waking up, when i run the code. I always needs to send 000h → 01 03 to wake him up via sniffer.
Hello Matt,
maybe the CANopen master boots faster than your PLC with X20IF1043-1. You can start the CANopen master with a delay. If that doesn’t help, please send a CAN trace from your sniffer where you can see the complete restart.
Gruß
Stephan
sample project created with Automation Studio 6
CanOpMa_6.zip (226.3 KB)