Custom widgets

This is a collection of customized widgets for mappView. The widgets are not officially development by B&R and have limited supported from the GitHub community. If you run into any issues with your mappView visualization and need to contact B&R support, please remove the custom widgets first to make sure the issue is not related to this widgets.

Link to Github

Kudos to @florent.boissadier for sharing his widgets

If you used the screenshot widget from this library, please make sure to update to version 7 of this widget. This version fixes a critical bug that could cause the T-Panels CPU load to go to 100%.

Are these all developed using the Widget development toolchain?

Here is a screenshot of the widgets list, just to catch the eye :slight_smile:

Yes, they were all developed with the tool chain. There is an extra branch for mappView version 5.20 and lower. I will port the widgets over to mappView 6.x later this week.

I may merge my OpcUacBrowser and my ThreeJSViewer just long enough to stabilize them and when the widgets will be port to mappView 6.x