When I finish compiling the programme and click the ‘Load’ button, I get the error shown in the photo.
This is the first time I’ve seen this, and I can’t find any information about this error in the B&R help section or online.
The programme is AS version 4.12.
Hi Ruben,
you compiled the project in Automation Studio, right?
What do you mean with the “Load” Button? The Transfer (to Target) Button in Automation Studio?
Do you have some messages in the output window of Automation Studio?
Did you try to:
Rebuild the project
Clean the temp folder of the project (while it is closed)
The customer saved AS prj in a folder in Synch with OneDrive. Could be your case?
When He moved the prj to C:\Temp no more issue.
================================
It’s not clear Ruben what you mean with “loading program“, in my case the customer got the same error every time He tried to build the prj.
I’m familiar with that message too, though only when using ArSim.
I work with ArSim a lot, and I’ve seen that message a few times during a (normal) transfer. (I think the message appears when the transfer window opens.)
My guess was also that some kind of file lock or something similar was causing it.
Restarting ArSim didn’t help back then, I don’t think I ever tried restarting the system (Windows).
However, after an offline installation, everything worked again, so I suspect the error was somewhere in the runtime directory (Temp-Folder).