When adding a new ACP10 Axis project, an error appears upon opening it: “‘REAL’ is an unexpected token. Expecting white space. Line 163.” Why is this happening?
Hi @boyu.zhu ,
similar issue was reported last year and below the answer from Support:
‘The problem occurs because of ANSI encoding used in the INIT Parameter XML Property Grid configuration. In this configuration are some unit definitions with “²” (e.g. Units/s²) which lead to the errors. If the “²” will be removed in the configuration the error does not occur any more.’
The issue is only with ACP10 and not with mapp Motion.