Eventscripts are not transferred Error

Hi B&R Community,

I recently changed the name of my alarmXcore configuration file and updated all of the MpLinks in the code to match the new link. After trying to build the project I get the following error: "Eventscripts are not transferred because the execution of event bindings has been configured to be executed on the server. Please set the execution to client in the mapp view configuration. "

I am trying to follow the error’s suggestion, but cannot find where to change the event bindings to ‘client’. Does anyone here know where I should look to access these configurations?

I am running Automation studio V6.7.0.187.

Hi Jessy,

This can be configured in the mappView server configuration file, which can be found in the Configuration View under the mappView folder.

Hi Tommi,

Thanks for the feedback. Should this option be available in automation studio V6.7.0.187? I do not see a config file inside my “mapp View” folder.

You can add it from the toolbox by selecting the mapp View folder and double clicking or dragging and dropping it to the mapp View folder.

I would suggest going through the getting started guide of mapp View.
mapp View - Getting started

Looks like I might have missed that. I no longer have the error, thanks Tommi!