I am using AS 3.0.90 with X20 1485-1. Why I can’t force the values of variables?
Hello,
For the handling of the Force Window i can not see an issue. The Force On is “grey out” because its context sensitive to the marked line (blue) which is already set so “force on”. This is why only the “force off” and “force all Off” is in “black” color.
I think you would more hint to the issue that all Variables show this “Error” in the PV Value column. Which also coresponds to the “warning triangle” at the begining of the line.
Normaly this is a hint, to have not the same Projekt Status than installed on the Machine.
Did you made shure the Project is matching the machine project?
Is it possible to allign Project an PLC with a Transfer?
Greetings
Michael
1 Like
Thank you! It was useful.