Github not showing any repositories

As some may have noticed our Github is not showing any public repositories.

We had a migration of our Github instance, this caused that no public repos are shown today. The public state should be corrected at the end of May.

Apologies for the inconvenience.

6 Likes

The “old” repos can be found under the following address

B&R Industrial Automation [Archive]

5 Likes

Hi @job.franken

Did this github will stay “open source” ?

Regards,
Florent

Yes, it will definitely stay open source. I hope it will be just a question of one or two more weeks to get them public again.

4 Likes

Hi @stephan.stricker,
Is there anny update about migration?
Are able to tel some forecast, when it will be done ?
Regards
Tomas

Unfortunately no, I asked DevOps today for an update. Remember, you can still access the repos under the archived address.

B&R Industrial Automation [Archive]

Yes, but lot links is target to br-automation repositry. Even here in commuity. So its making confusion in costumers.

Is it possible to make pull requests in B&R Industrial Automation [Archive]?
For example link for documetation (docosaurus) for X20-Edge-UseCases is using br-automation repostiory,

Unfortunatly you cannot make pull request, all repos are in read-only :confused:

1 Like

I don’t think it is possible to make pull request against achieved repos as well as new commits. So we hope that this gets resolved soon. Documentation follows the same pattern as the repos. You have to add “archive-” in front of the URL. For the edge device, the archived link is this:

B&R X20 Edge Use Cases | B&R X20 Edge

Thank for info.
ps.: About documetation,I already figured it out. :slight_smile:

I see there is a link here:

Archived - To continue, use: ABB-EMU: Sign in to ABB-EMU · GitHub

Is this how to access the updated repos? Will there be public access?

I’m not sure about the current state, but if I’m not mistaken, GitHub repositories will have public access soon.

Unfortunately the GitHub repos are still not public but the latest information from IT suggests that it should be back online first week of July.

2 Likes

The public repos are back only under the following address

B&R Industrial Automation [Public]

9 Likes

We have run the script to rename the old GitHub URL “Sign in to ABB-EMU · GitHub” to the new one “B&R Industrial Automation [Public] · GitHub”, so all URL links in all discussions should be updated and the repository should again be accessible. If you find a link that is not updated, please let me know.

5 Likes