How to backup from acoposinverter p84

Good morning,

This is Mohsen. I’m going to get a backup from the ACOPOS inverter P84 without a CF card via software. Please help me with how to get the backup and what software I need.

Good morning @mohsen.bashiri ,

If the ACOPOSinverter is operated on a B&R controller (which is the recommended method), then all the controller parameters are known to the PLC and stored on its flash.
A fresh ACOPOSinverter connected to this PLC would be automatically set up via network.

If the ACOPOSinverter instead is operated stand-alone, it is possible to save/load the parameters in the optional graphic display (Load/Save As).

Regards,