How to restore previous security behavior after migration from AS4 to AS6

Several security settings will be enforced after the migration. While we do recommend using the new settings for improved security, here are the steps to restore the previous behavior:

Restoring Previous Security Behavior After Migration


1. Allow access without a certificate

Change the following settings in the OPC Client/Server configuration
(Configuration View → Connectivity → OpcUaCs → UaCsConfig.uacfg):

ClientServerConfiguration -> Security -> MessageSecurity -> SecurityPolicies -> None: Enabled

2. Enable anonymous access instead of user login

Change the following settings in the mappView configuration
(Configuration View → mappView → Config.mappviewcfg):

MappViewConfiguration -> Server Configuration -> Startup User: anonymous token

3. Enable anonymous authentication in OPC Client/Server

Change the following settings in the OPC Client/Server configuration
(Configuration View → Connectivity → OpcUaCs → UaCsConfig.uacfg):

  • Click the two green blocks at the top labeled “Change Advanced Parameter Visibility”
  • Enable the following:
ClientServerConfiguration -> Security -> Authentication -> Authentication Methods -> Anonymous: Enabled

ClientServerConfiguration -> Security -> Authorization -> AnonymousAccess -> User Role 1: Everyone

4. Configure the user role system for anonymous access

Change the following settings in the User Role System
(Configuration View → AccessAndSecurity → UserRoleSystem → User.user):

  • Assign the role “BR_Engineer” to the user “Anonymous”
  • If the user does not already exist, create it without a password

5. Whitelist a File Device for mappView access

To allow access to a File Device from a running mappView application, you must explicitly whitelist it:

  1. Open the mappView server configuration file
    2.(Configuration View → mappView → Config.mappviewcfg)*
  2. Click “Change Advanced Parameter Visibility” in the editor toolbar
  3. Enter the accessed File Device Name under:
MappViewConfiguration -> Server configuration -> File device whitelist
7 Likes