Hypervisor failed boot after installation

Hi, just to be sure: the USB key for booting is plugged into a USB port which is assigned to ARembedded?

Hi, yes the USB key is plugged to one of the two USB ports, which are assigned to ARembedded.

Hi Philipp, what is status of your topic, have you investigated anything? can you update us?

Sorry, as of now the problem could not be solved.

Did you get in contact with local support? I think they can connect to you and check your settings with you. Please share with us a solution if you find one.

closed due to inactivity. Can be reopened anytime if additional discussion is needed.

hi guys,
I got the exact same problem here.
had tried many times…very fraustrated…

if I manually switch to windows from menu, it will always be a error.

log.txt as below
Real-Time Hypervisor
Copyright 2006 - 2021 Real-Time Systems GmbH
Version R5.4.06.28286

Init CPU
Init heap
Init registry
Read configuration
First line in file must start with
“# RTH CONFIG” and only ASCII printable and white space characters are allowed in file.
ERR: 00000045 | 586507E0 | 00000000 | 00000000 | 00000000 | 00000000 | 01008587
No valid configuration file found.
ERR: 00000075 | 5F0456E8 | 00000000 | 00000000 | 00000000 | 01000197 | 01008492
Hypervisor boot failed.




install_log.zip (7.3 KB)

hi friends

It’s my fault. i choose wrong PLC type. KBU2 instead of KBU0.
thanks the support from B&R team here.

I just troubleshooted the same exact issue with a customer, and want to add that the culprit can also be the Automation Panel. In their case, they had a PPC900 with an AP933, but in AS they had configured an AP1120 for the panel. Once replacing the hardware module with the correct one in the Physical View, rebuilding, creating a new USB install image, and installing via BIOS on the PPC900, Hypervisor installed without issue.