I have a project where we use F:\ on the PLC to store a configuration file for the machine I’m working on. We’re using an APC3100 with AR only.
After installing my project on the PLC, I’ll use a FTP client to transfer the configuration file to the PLC.
I wonder if it is possible to include my configuration file in the installation package that I create when performing an offline installation?
Best regards
/Johnny
You can do this by using the “Automatic transfer of user files” configuration. Instructions can be found in Automation Help, link below.
Automation Help: Synchronizing user files
Interesting! Does this information also applies if I’m using F:\ on the PLC instead of an user partition on C:\ ?
The files are always transferred to the root of the User Partition (F:). The folder you choose in the dialog is the location of the files on your computer.
As a tip it can be inside the Automation Studio project and I usually create a “UserFiles” package to the project and the folder structure required by the project inside this package.
Ok, thanks. I will try this!
No wait a minute, this only applies if you do a transfer, right?
My question was about including a user file in a project installation package. I need to do the initial installation from an USB.
They are also included in the PIP package